Command/Query
:CALCulate:TRACe{Tr}:MARKer{Mk}:X <numeric>
:CALCulate:TRACe{Tr}:MARKer{Mk}:X?
This command sets stimulus value of the marker.
|
Description |
Marker stimulus value (X-Axis) |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
- |
|
Preset Value |
-10n |
|
Unit |
- |
|
Resolution |
- |
{numeric}<newline><^END>
10 OUTPUT 717;":CALC:TRAC1:MARK1:X 50"
20 OUTPUT 717;":CALC:TRAC1:MARK1:X?"
30 ENTER 717;A
:CALCulate:TRACe{Tr}:MARKer{Mk}:Y
Setup > Advanced Mode > Marker > Select Marker (Entry box above the graph plot)